1.3.3.27 SYS_NET_GetStatus Function
C
SYS_NET_STATUS SYS_NET_GetStatus ( SYS_MODULE_OBJ object )
Summary
Returns System NET instance status.
Description
This function returns the current status of the System NET instance.
Precondition
SYS_NET_Open should have been called before calling this function
Parameters
| Param | Description |
|---|---|
| object | SYS NET object handle, returned from SYS_NET_Open |
Returns
SYS_NET_STATUS
Example
// Handle "objSysNet" value must have been returned from SYS_NET_Open.
if (SYS_NET_GetStatus (objSysNet) == SYS_NET_STATUS_SERVER_AWAITING_CONNECTION)
{
// NET system service is initialized and the NET server is ready to accept new connection.
}Remarks
None.