1.3.3.28 SYS_NET_RecvMsg Function
C
int32_t SYS_NET_RecvMsg(SYS_MODULE_OBJ obj, void *data, uint16_t len)Summary
Returns No of Bytes received from peer using the System NET instance.
Description
This function returns the number of bytes received from the peer.
Precondition
SYS_NET_Open should have been called.
Parameters
obj - SYS NET object handle, returned from SYS_NET_Open data - valid data buffer pointer len - length of the data to be transmitted
Returns
SYS_NET_SERVICE_DOWN - Indicates that the System NET instance is not connected to the peer
SYS_NET_GET_NOT_READY - Indicates that the System NET instance No Data to GET
Positive Non-Zero - Indicates the number of bytes received from the peer, which may be less than the "len" of the buffer passed as the param.
Example
// Handle "objSysNet" value must have been returned from SYS_NET_Open. int32_t len = 32; uint8_t buffer[32] = {0}; len = SYS_NET_RecvMsg(objSysNet, buffer, len); if(len > 0) { }
Remarks
None.