12.2.3 Why Disable Interrupts
Global interrupts must be disabled while a peripheral is unlocked as an interrupt handler would not know the current state of the peripheral lock. If the interrupt tries to alter the lock state, it can cause an exception as it potentially tries to unlock an already unlocked peripheral. Reading current lock state is to be avoided as it removes the security provided by the PAC (Reading Lock State).
Note: Global interrupts should also be disabled when a peripheral is unlocked inside an interrupt handler.
An example to illustrate the potential hazard of not disabling interrupts is shown in Figure 12-2.