12.2.6 Use of __no_inline
Using the function attribute __no_inline will ensure that there will only be one copy of each functions in the PAC driver API in the application. This will lower the likelihood that runaway code will hit any of these functions.