29.6.3.3.1 Function rww_eeprom_emulator_write_buffer()
Writes a buffer of data to the emulated RWW EEPROM memory space.
enum status_code rww_eeprom_emulator_write_buffer( const uint16_t offset, const uint8_t *const data, const uint16_t length)
Writes a buffer of data to a section of emulated RWW EEPROM memory space. The source buffer may be of any size, and the destination may lie outside of an emulated RWW EEPROM page boundary.
| Data direction | Parameter name | Description |
|---|---|---|
|
[in] |
offset |
Starting byte offset to write to, in emulated RWW EEPROM memory space |
|
[in] |
data |
Pointer to the data buffer containing source data to write |
|
[in] |
length |
Length of the data to write, in bytes |
Returns
Status code indicating the status of the operation.
| Return value | Description |
|---|---|
|
STATUS_OK |
If the page was successfully read |
|
STATUS_ERR_NOT_INITIALIZED |
If the RWW EEPROM emulator is not initialized |
|
STATUS_ERR_BAD_ADDRESS |
If an address outside the valid emulated RWW EEPROM memory space was supplied |