Error code bit field reports the status of the last programming operation.
INVALIDCMD and WRITEPROTECT are cleared
only if/whenthe operation that caused the error is followed by a legal one. If
CMDCOLLISION error occurs, then any new programming
operation is ignored, until the error is cleared. Ensure no programming
operation is ongoing (see FBUSY and EEBUSY flags) before clearing this error,
otherwise the error will be reported once more.
The Error Code bit field can be cleared by writing ‘0’ to it.
Note: Rules for error/halting:
- If changing command while
programming is ongoing, then
CMDCOLLISION error is
set.
- If ERROR =
CMDCOLLISION, then the programming operation is
ignored.
- If accessing (read/write)
while NVM section is busy, then the CPU is halted.
| Value | Name | Description |
|---|
| 0x0 |
NONE |
No
error |
| 0x1 |
INVALIDCMD |
The
selected command is not supported |
| 0x2 |
WRITEPROTECT |
Attempt
to write a section that is protected |
| 0x3 |
CMDCOLLISION |
A new
write/erase command was selected while a write/erase command was already
ongoing |
| Other |
— |
Reserved |