5.3 Place and Route
(Ask a Question)To place and route, perform the following steps:
- On the Design Flow tab, double-click Place and Route, a green tick mark appears as shown in Figure 5-3.
- To view I/O Editor in Transceiver view, on the Design Flow tab, double-click Manage Constraints.
- On the I/O Attributes tab, from the Edit drop-down list, click Edit with I/O Editor.
- In the I/O Editor, open XCVR View.
For DFE design, TX_PLL, XCVR_REF_CLK, and XCVR are constrained using the I/O Editor as shown in the following figure.