3.2.1.1 DDR Memory Partition
(Ask a Question)The following figure shows the memory mapping of the 2 GB on-board DDR memory in the Linux device tree.
PolarFire SoC video kits come with 2 GB of DDR memory by default, partitioned as follows:
- 2 GB of DDR memory is mapped as listed:
- 1 GB 32-bit cached memory at 0✕80000000
- 256 MB 32-bit non cached memory at 0✕C0000000
- 2 GB 64-bit cached memory at 0✕1000000000
- 2 GB 64-bit non-cached memory at 0✕1400000000
The following figure shows the settings used in the design.