3.2.1 DDR Memory Mappings
(Ask a Question)This section describes the DDR regions and their allocations. It also explains how these memory regions are defined in the Linux device tree so that the Linux user space can address these regions.
For more information about DDR memory partition regions, see the “Segmentation Blocks” section in PolarFire SoC MSS Technical Reference Manual.