5.9.4.5 OTA File Read SPI
NMI_API sint8 m2m_ota_host_file_read_spi
(
uint8 u8Handler,
uint8 *pu8Buff,
uint32 u32Offset,
uint32 u32Size
);
The file read via SPI is similar to the read via HIF. The use of a callback is not considered, because to access the WINC’s Flash via SPI, the WINC must be set into a certain mode to allow for safe read/write of its Flash. Therefore, it is typical to use a loop to read all the data necessary while the WINC is in that state and then restart the WINC.
To use this API, the application must call
m2m_wifi_download_mode to make the WINC safe for read/write Flash
access and once the read is completed, the WINC must be reinitialized
(m2m_wifi_reinit, m2m_ota_init) and to connect to
the network again if the Application based on the request. pu8Buff is a
pointer to a buffer provided by the Application and to where the data will be read
to.
Advantages (vs HIF read)
- SPI read is faster than HIF Read.
Disadvantages (vs HIF read)
- Requires the WINC to set into a special mode and restart later.
- Generally blocks as the read are done within a loop to minimize WINC reset.