8.5 AP Mode Code Example
The following example shows how to configure the
ATWINC15x0 AP mode with
WINC_SSID as broadcasted SSID on channel one with open security and
an IP address equals 192.168.1.1.
#include "m2m_wifi.h"
#include "m2m_types.h"
void wifi_event_cb(uint8 u8WiFiEvent, void * pvMsg)
{
switch(u8WiFiEvent)
{
case M2M_WIFI_REQ_DHCP_CONF:
{
uint8 *pu8IPAddress = (uint8*)pvMsg;
printf("Associated STA has IP Address \"%u.%u.%u.%u\"\n", pu8IPAddress[0],
pu8IPAddress[1], pu8IPAddress[2], pu8IPAddress[3]);
}
break;
default:
break;
}
}
int main()
{
tstrWifiInitParam param;
/* Platform specific initializations. */
param.pfAppWifiCb = wifi_event_cb;
if (!m2m_wifi_init(¶m))
{
tstrM2MAPConfig apConfig;
strcpy(apConfig.au8SSID, "WINC_SSID"); // Set SSID
apConfig.u8SsidHide = SSID_MODE_VISIBLE; // Set SSID to be broadcasted
apConfig.u8ListenChannel = 1; // Set Channel
apConfig.u8SecType = M2M_WIFI_SEC_WEP; // Set Security to WEP
apConfig.u8KeyIndx = 0; // Set WEP Key Index
apConfig.u8KeySz = WEP_40_KEY_STRING_SIZE; // Set WEP Key Size
strcpy(apConfig.au8WepKey, "1234567890"); // Set WEP Key
// IP Address
apConfig.au8DHCPServerIP[0] = 192;
apConfig.au8DHCPServerIP[1] = 168;
apConfig.au8DHCPServerIP[2] = 1;
apConfig.au8DHCPServerIP[3] = 1;
// Start AP mode
m2m_wifi_enable_ap(&apConfig);
while(1)
{
m2m_wifi_handle_events(NULL);
}
}
}
Note: Power Save mode is not supported in the
ATWINC15x0 AP mode.