9.3.1 WPS Configuration Methods
There are two authentication methods that can be used with WPS:
- PBC (push button) method – A physical
button is pressed on the AP which puts the AP into WPS mode for a limited period of
time. WPS is initiated on the ATWINC15x0 by calling
m2m_wifi_wpswith input parameterWPS_PBC_TRIGGER. - PIN method – The AP is always
available for WPS initiation but requires proof that the user has knowledge of an
8-digit PIN, usually printed on the body of the AP. Since the WINC is often used in
headless devices (no user interface), it is necessary to reverse this process and
force the AP to use a PIN number provided with the WINC device. Some APs allow the
PIN to be changed through configuration. WPS is initiated on the ATWINC15x0 by calling
m2m_wifi_wpswith input parameterWPS_PIN_TRIGGER. Given the difficulty of this approach, it is not recommend for most applications.
The flow of messages and actions for WPS operation is shown in the following figure.