1.9.10.7 FCW_ErrorGet Function

C

FCW_ERROR FCW_ErrorGet( void )

Summary

Returns the error state of FCW controller.

Description

This function returns the erorr status of the last FCW operation.

Precondition

None.

Parameters

None

Returns

Return FCW_ERROR type of value. In case of error, this value can be a combination of multiple and different error conditions.

Example

if(FCW_ErrorGet() != FCW_ERROR_NONE)
{
    // The error status can indicate multiple error conditions.
    if(FCW_ErrorGet() & (FCW_ERROR_WRITE | FCW_ERROR_RESET))
    {
        // There are multiple error conditions.
    }
}

Remarks

None.