1.9.10.4 FCW_SingleDoubleWordWrite Function

C

bool FCW_SingleDoubleWordWrite( uint32_t *data, uint32_t address );

Summary

Writes Two Words into the Flash.

Description

Writes Two Words (8 bytes) at the given address.

Precondition

None

Parameters

Param Description
data Pointer to the buffer which holds data to be written.
address Address at which the data will be written.

Returns

Always return true.

Example

uint32_t data[2];

data[0] = 0x12345678;
data[1] = 0x87654321;

FCW_SingleDoubleWordWrite((uint32_t *)data, 0xC088608U);

Remarks

This Feature may not be available on all devices. Refer to device Datasheet for more information.