1.26.5.28 FLEXCOM_USART_RING_BUFFER_CALLBACK Typedef
C
/* Ring buffer mode */ typedef void (* FLEXCOM_USART_RING_BUFFER_CALLBACK)(FLEXCOM_USART_EVENT event, uintptr_t context )
Summary
Defines the data type and function signature for the FLEXCOM_USART peripheral callback function in the ring buffer mode
Description
This data type defines the function signature for the FLEXCOM_USART peripheral callback function in the ring buffer mode. The FLEXCOM_USART peripheral will call back the client's function with this signature when the FLEXCOM_USART buffer read/write event has occurred.
Precondition
FLEXCOMx_USART_Initialize must have been called for the given FLEXCOM_USART peripheral instance. Callback must have been registered using FLEXCOMx_USART_WriteCallbackRegister or FLEXCOMx_USART_ReadCallbackRegister routines and event notifications are enabled using the FLEXCOMx_USART_WriteNotificationEnable or FLEXCOMx_USART_ReadNotificationEnable routines.
Parameters
Param | Description |
---|---|
event | Indicates the event for which the callback is called |
context | Allows the caller to provide a context value (usually a pointer to the callers context for multiple clients). |
Returns
None.
Example
uint8_t txBuffer[50]; uint8_t rxBuffer[10]; volatile bool txThresholdEventReceived = false; volatile bool rxThresholdEventReceived = false; volatile uint32_t nBytesRead = 0; void usartWriteEventHandler(FLEXCOM_USART_EVENT event, uintptr_t context ) { txThresholdEventReceived = true; } void usartReadEventHandler(FLEXCOM_USART_EVENT event, uintptr_t context ) { uint32_t nBytesAvailable = 0; if (event == FLEXCOM_USART_EVENT_READ_THRESHOLD_REACHED) { nBytesAvailable = FLEXCOM0_USART_ReadCountGet(); nBytesRead += FLEXCOM0_USART_Read((uint8_t*)&rxBuffer[nBytesRead], nBytesAvailable); } } //----------------------------------------------------------// // Register a callback for write events FLEXCOM0_USART_WriteCallbackRegister(usartWriteEventHandler, (uintptr_t) NULL); // Set TX threshold - TX buffer is empty FLEXCOM0_USART_WriteThresholdSet(FLEXCOM0_USART_WriteBufferSizeGet()); // Enable notifications. Enables notification when threshold condition is reached FLEXCOM0_USART_WriteNotificationEnable(true, false); // Register a callback for read events FLEXCOM0_USART_ReadCallbackRegister(usartReadEventHandler, (uintptr_t) NULL); // Set RX threshold - when 5 characters are available in the receive buffer FLEXCOM0_USART_ReadThresholdSet(5); // Enable RX event notifications FLEXCOM0_USART_ReadNotificationEnable(true, false);
Remarks
None.