1.1.4.35 GPIO_INP_READ Enum

C

The GPIO_INP_READ vary based on device family. Refer to the generated header file for the actual values.

Summary

This enum is used to enable or disable input for a pin using the GPIO_PinInputConfig API

Description

This enum is used to enable or disable input for a pin using the GPIO_PinInputConfig API

Remarks

None