1.1.4.25 void GPIO_PinSlewRateConfig(GPIO_PIN pin, GPIO_SLEW_RATE slewRate) Function

C

void GPIO_PinSlewRateConfig(GPIO_PIN pin, GPIO_SLEW_RATE slewRate)

Summary

Configures the slew rate on the given GPIO pin

Description

This API lets the application configure the slew rate on the given GPIO pin

Precondition

None

Parameters

Param Description
pin One of the values from the enum GPIO_PIN
slewRate One of the values from the enum GPIO_SLEW_RATE

Returns

None

Example

GPIO_PinSlewRateConfig(GPIO_PIN_GPIO012, GPIO_SLEW_RATE_FAST);

Remarks

None