1.1.4.7 void GPIO_PinGroupOutputDisable(GPIO_PIN pin) Function

C

void GPIO_PinGroupOutputDisable(GPIO_PIN pin)

Summary

Disables the group output of the given GPIO pin

Description

Every GPIO has two mechanisms to set a GPIO data output - either using the grouped GPIO output register or using the single GPIO output data bit located in the Pin Control register. This API disables control of the GPIO pin using the grouped GPIO output register (and hence enables control using the Pin Control register)

Precondition

None.

Parameters

Param Description
pin One of the GPIO pins from the enum GPIO_PIN

Returns

None

Example

GPIO_PinGroupOutputDisable(GPIO_PIN_GPIO012);

Remarks

None