1.1.4.28 void GPIO_DrvStrConfig(GPIO_PIN pin, GPIO_DRV drvStrn) Function

C

void GPIO_DrvStrConfig(GPIO_PIN pin, GPIO_DRV drvStrn)

Summary

Configures the drive strength on the given GPIO pin

Description

This API lets the application configure the drive strength on the given GPIO pin

Precondition

None

Parameters

Param Description
pin One of the values from the enum GPIO_PIN
drvStrn One of the values from the enum GPIO_DRV

Returns

None

Example

GPIO_DrvStrConfig(GPIO_PIN_GPIO012, GPIO_DRV_STR_LEVEL1);

Remarks

None