1.32.25.9 SDHCx_ErrorReset Function

C

/* x = SDHC instance number (x is applicable only on devices with more than one instances of SDHC) */

void SDHCx_ErrorReset ( SDHC_RESET_TYPE resetType )

Summary

Resets errors as specified by the resetType

Description

Resets errors as specified by the resetType

Precondition

SDHCx_Initialize() must have been called first for the associated instance.

Parameters

Param Description
resetType Type of error to reset

Returns

None.

Example

SDHC1_ErrorReset(SDHC_RESET_ALL);

Remarks

None.