1.32.25.3 SDHCx_ModuleInit Function
C
/* x = SDHC instance number (x is applicable only on devices with more than one instances of SDHC) */ void SDHCx_ModuleInit ( void )
Summary
Initializes the SDHC peripheral.
Description
This function initializes the SDHC peripheral. The SDHC peripheral is initialized in 1 bit mode and the SDHC clock is set to 400 kHz. This function may be called at run time to re-initialize the peripheral to the initial state.
Precondition
None.
Parameters
None.
Returns
None.
Example
SDHC1_ModuleInit();
Remarks
None.