1.8.19.25 SEFCx_UserSignatureRightsSet Function

C

void SEFCx_UserSignatureRightsSet(uint32_t userSignatureRights);

Summary

Writes the access rights of the user signature

Description

This function writes the access rights of the user signature

Precondition

None.

Parameters

Param Description
userSignatureRights rights of the user signature

Returns

None.

Example

 uint32_t usrRights = SEFC0_UserSignatureRightsGet();
 usrRights |= (SEFC_EEFC_USR_RDENUSB1_Msk | SEFC_EEFC_USR_WRENUSB1_Msk);
 SEFC0_UserSignatureRightsSet(usrRights);

Remarks

None.