2.81.5 PIO_PortSet Function
C
void PIO_PortSet(PIO_PORT port, uint32_t mask)
Summary
Set the selected IO pins of a port.
Description
This function sets (to '1') the selected IO pins of a port.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| port | One of the IO ports from the enum PIO_PORT |
| mask | A 32 bit value in which positions of 0s and 1s decide which IO pins of the selected port will be set. |
-
1's Will set corresponding IO pins to high (to 1).
-
0's Will remain unchanged.
Returns
None.
Example
// Set PC5 and PC7 pins to 1 PIO_PortSet(PIO_PORT_C, 0x00A0);
Remarks
If the port has less than 32-bits, unimplemented pins will be ignored. Implemented pins are Right aligned in the 32-bit value.