2.81.13 PIO_PinRead Function
C
bool PIO_PinRead(PIO_PIN pin)
Summary
Read the selected pin value.
Description
This function reads the selected pin value. it reads the value regardless of pin configuration, whether uniquely as an input, or driven by the PIO Controller, or driven by peripheral.
Precondition
Reading the I/O line levels requires the clock of the PIO Controller to be enabled, otherwise this API reads the levels present on the I/O line at the time the clock was disabled.
Parameters
| Param | Description |
|---|---|
| pin | One of the IO pins from the enum PIO_PIN |
Returns
Returns the read value of the selected I/O pin.
Example
bool value; value = PIO_PinRead(PIO_PIN_PB3);
Remarks
To read the latched value on this pin, PIO_PinLatchRead API should be used.