2.133.22 XDMAC_MICRO_BLOCK_CONTROL Struct
C
typedef struct {
/* Size of block for the current descriptor. */
uint32_t blockDataLength:24;
/* Next Descriptor Control Setting */
XDMAC_DESCRIPTOR_CONTROL nextDescriptorControl;
} XDMAC_MICRO_BLOCK_CONTROL;
Summary
Defines the control parameters for linked list operation.
Description
This data type defines the control parameters for linked list operation. Block length applies to the current descriptor and XDMAC_DESCRIPTOR_CONTROL applies to the next descriptor.
Remarks
This feature may not be available on all devices. Refer to the specific device data sheet to determine availability.