2.127.8 TSENS_ConversionResultGet Function

C

uint32_t TSENS_ConversionResultGet(void);

Summary

Returns the measured temperature value

Description

This function returns the last measured temperature value.

Precondition

TSENS_Initialize() function must have been called first for the associated instance

Parameters

None

Returns

result - 24-bit last measured temperature value

Example

uint32_t result;
TSENS_Initialize();
TSENS_Enable();
TSENS_ConversionStart();
while(!TSENS_ConversionStatusGet());
result = TSENS_COnversionResultGet();

Remarks

This function can be called from interrupt or by polling the status when result is available. The result is 24-bit value in two's complement format.