2.127.12 TSENS_WindowMonitorStatusGet Function
C
bool TSENS_WindowMonitorStatusGet(void);
Summary
Read the status of the window monitor comparison
Description
This function returns the status of the comparison of measured temperature and the predefined window threshold values
Precondition
TSENS_Initialize() function must have been called first for the associated instance
Parameters
NoneReturns
true - when measured temperature satisfies the window mode and threshold values
false - when measured temperature is out of range
Example
bool status = false; TSENS_Initialize(); TSENS_Enable(); TSENS_ConversionStart(); status = TSENS_WindowMonitorStatusGet();
Remarks
This function is used to poll the window comparison status. This should be called after conversion is started.