2.5.8 AFECx_ChannelResultGet Function
C
uint16_t AFECx_ChannelResultGet (AFEC_CHANNEL channel) // x - Instance of the AFEC peripheral
Summary
Reads the conversion result of the channel
Description
This function reads the conversion result of the channel
Precondition
AFECx_Initialize() must have been called first for the associated instance. And conversion must have been started.
Parameters
| Param | Description |
|---|---|
| channel | channel number |
Returns
uint16_t - conversion result
Example
uint16_t result;
bool status;
AFEC0_Initialize();
AFEC0_ChannelsEnable(AFEC_CH0);
AFEC0_ConversionStart();
status = AFEC0_ChannelResultIsReady(AFEC_CH0);
if (status)
{
result = AFEC0_ChannelResultGet(AFEC_CH0);
}
Remarks
This function can be called from interrupt or by polling the status when result is available. User should decode the result based on result sign mode (signed or unsigned result) and result resolution (12, 13, 14, 15 or 16 bit result) configuration.