2.5.9 AFECx_ConversionSequenceSet Function
C
void AFECx_ConversionSequenceSet (AFEC_CHANNEL *channelList, uint8_t numChannel) // x - Instance of the AFEC peripheral
Summary
Sets the user sequence of the channel conversion
Description
This function sets the order in which channels are converted.
Precondition
AFECx_Initialize() must have been called first for the associate instance. Conversion should not be ongoing while changing the sequence.
Parameters
| Param | Description |
|---|---|
| *channelList | pointer to the list of the channels which describes the order of conversion |
| numChannel | Number of enabled channels in the list |
Returns
None.
Example
AFEC_CHANNEL seq_order[4] = {AFEC_CH3, AFEC_CH5, AFEC_CH1, AFEC_CH2}; AFEC0_Initialize(); AFEC0_ConversionSequenceSet(seq_order, 0x4); AFEC0_ChannelsEnable(AFEC_CH0_MASK | AFEC_CH1_MASK | AFEC_CH2_MASK | AFEC_CH3_MASK);
Remarks
Conversion order is set in this function and remains valid until user configures new conversion sequence order or reinitializes the peripheral. Array pointed to by *channelList must be valid during the call to this function. This function copies the array data into AFEC HW registers.