2.65.6 MCPWM_PrimaryPeriodGet Function
C
uint16_t MCPWM_PrimaryPeriodGet (void)
Summary
Reads the period value of primary time base generator
Description
This function reads the period value of primary time base generator
Precondition
MCPWM_Initialize() function must have been called first for the associated instance.
Parameters
None
Returns
The MCPWM primary time base period value
Example
uint16_t period; MCPWM_Initialize(); period = MCPWM_PrimaryPeriodGet();
Remarks
None