2.65.8 MCPWM_ChannelPrimaryDutySet Function
C
void MCPWM_ChannelPrimaryDutySet(MCPWM_CH_NUM channel, uint16_t duty)
Summary
Writes the primary duty cycle value of given MCPWM channel
Description
This function writes the primary duty cycle value
Precondition
MCPWM_Initialize() function must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
channel | MCPWM channel number |
duty | duty cycle value which determines ON time of waveform |
Returns
None
Example
MCPWM_Initialize(); MCPWM_Start(); MCPWM_ChannelPrimaryDutySet(MCPWM_CH_0, 0x200);
Remarks
In edge-aligned mode, this specifies the trailing edge of the ON time. In center-aligned mode, this specifies the leading edge transition.