3.12.19.12 SEFC_RegionLock Function
C
void SEFC_RegionLock(uint32_t address);
Summary
Locks a Flash region.
Description
This function takes an address as a parameter and locks the region associated with it.
Precondition
Validate if SEFCx controller is ready to accept new request by calling SEFC_IsBusy()
Parameters
| Param | Description |
|---|---|
| address | Address of the page to be locked |
Returns
None.
Example
SEFC_RegionLock(0x00500000); while(SEFC_IsBusy(0x00500000));