3.12.19.8 SEFC_PageErase Function
C
bool SEFC_PageErase( uint32_t address)
Summary
Erases a Page in the FLASH.
Description
Depending on which flash panel is mapped at the given address, it calls the associated SEFC flash controller instance and erases the corresponding page.
Precondition
Validate if SEFCx controller is ready to accept new request by calling SEFC_IsBusy()
Parameters
| Param | Description |
|---|---|
| address | FLASH address to be Erased |
Returns
Always returns true.
Example
SEFC_PageErase(0x500000); while(SEFC_IsBusy(0x500000));
Remarks
Application needs to poll for busy bit or wait for callback to be called before sending next request.