3.12.19.11 SEFC_PageWrite Function
C
bool SEFC_PageWrite( uint32_t* data, uint32_t address )
Summary
Writes data of size equivalent to page size to a given FLASH address.
Description
This function takes a 32-bit address and a pointer to page-sized data. Depending on which flash panel is mapped at the given address, it calls the associated SEFCx flash controller instance and writes the data to the give location in FLASH.
Precondition
Validate if SEFCx controller is ready to accept new request by calling SEFC_IsBusy() The Page to be written should be in Erased State.
Parameters
| Param | Description |
|---|---|
| address | FLASH address to be modified |
| data | pointer to data buffer |
Returns
Always returns true.
Example
SEFC_PageWrite( (uint32_t *) buffer, 0x500000); while(SEFC_IsBusy(0x500000));
Remarks
Application needs to poll for busy bit or wait for callback to be called before sending next request.