3.12.19.14 SEFC_SectorErase Function
C
bool SEFC_SectorErase( uint32_t address)
Summary
Erases a Sector in the FLASH.
Description
This function determines the flash panel for the given address by calling `SEFC_FlashPanelGet` and then erases the corresponding sector (collection of pages).
Precondition
Validate if SEFCx controller is ready to accept new request by calling SEFC_IsBusy()
Parameters
| Param | Description |
|---|---|
| address | FLASH address to be Erased |
Returns
Always returns true.
Example
SEFC_SectorErase(0x500000);
while(SEFC_IsBusy());
Remarks
Application needs to poll for busy bit or wait for callback to be called before sending next request.