2.53.4 HEMC_EnableECC Function
C
bool HEMC_EnableECC( uint8_t chipSelect )
Summary
Enable the ECC for the given chip select.
Description
This function enable the ECC for the given chip select of the HEMC peripheral.
Precondition
None.
Parameters
Param | Description |
---|---|
chipSelect | The chip select for which ECC is enabled. |
Returns
True if ECC was enable for this chip select, False otherwise.
Example
HEMC_EnableECC(0);
Remarks
None.