3.4.2 Analog-to-Digital Converter (ADC)
-
Up to 12-bit resolution of the numerical output, signed or unsigned
-
Signed outputs left- or right-adjusted
-
Up to 5.14 Msps conversion rate per channel
-
Up to 4 Shared Analog ADC SAR cores (bound by limited CSR and pin-out resources) for an aggregate conversion rate of 20.5 Msps per entire ADC module by performing up to 4 conversions simultaneously
-
Up to 64 analog inputs (maximum of 16 channels per core).
-
Single-ended and/or differential inputs on a per channel basis for all channels.
-
Up to 16 trigger sources, off-chip hardware or on-chip hardware or software generated
-
Edge or level active triggering modes, to generate single conversions or bursts of conversions
-
A scan trigger per each shared Analog ADC SAR Core to start a scan cycle which can individually include or not any of the analog inputs assigned to that Analog ADC SAR Core
-
Up to 4 scan cycles running simultaneously
-
Any channel can select any of the 16 trigger sources or the scan trigger as its own trigger
-
The scan trigger itself can select any of the 16 trigger sources as its own source Programmable sampling time, individual for each shared Analog ADC SAR Core
-
Each analog input / channel output register can be read from an general dedicated APB output register (user writes the CORDYID and CHRDYID then reads the CHRDYDATA register).
Using The Library
Interrupt mode:
#include <stddef.h> // Defines NULL #include <stdbool.h> // Defines true #include <stdlib.h> // Defines EXIT_FAILURE #include "definitions.h" // SYS function prototypes #define ADC_VREF (3.3f) volatile uint32_t adc_data[3]; volatile bool adc_sequence_done = false; volatile bool adc_ch2_done = false; float adc_inp_vol; // ***************************************************************************** // ***************************************************************************** // Section: Main Entry Point // ***************************************************************************** // ***************************************************************************** void ADC_EventHandler(ADC_CORE_INT status, uintptr_t context) { /* ADC1_CH0 and ADC1_CH1 are configured for scan trigger */ if (status & ADC_CORE_INT_EOSRDY) { adc_data[0] = ADC_ResultGet(ADC_CORE_NUM1, ADC_CH0); adc_data[1] = ADC_ResultGet(ADC_CORE_NUM1, ADC_CH1); adc_sequence_done = true; } /* ADC1_CH2 is configured for Global (Edge) Software trigger */ if (status & ADC_CORE_INT_CHRDY_2) { adc_data[2] = ADC_ResultGet(ADC_CORE_NUM1, ADC_CH2); adc_ch2_done = true; } } int main ( void ) { /* Initialize all modules */ SYS_Initialize ( NULL ); printf("\r\n *********************************************** \r\n"); printf("\r\n ADC INTERRUPT DEMO \r\n"); printf("\r\n *********************************************** \r\n"); ADC_CORE1CallbackRegister(ADC_EventHandler, 0); RTC_Timer32Start(); while ( true ) { if (SWITCH_Get() == 0) { // Wait for switch release while (SWITCH_Get() == 0); ADC_GlobalEdgeConversionStart(); } if (adc_sequence_done == true) { adc_sequence_done = false; adc_inp_vol = (uint16_t)adc_data[0] * ADC_VREF / 4095U; printf("\r\n ADC1_AIN0: ADC Count: 0x%03x, ADC Input Voltage = %d.%02d V \r\n", (uint16_t)adc_data[0], (int)adc_inp_vol, (int)((adc_inp_vol - (int)adc_inp_vol)*100.0)); adc_inp_vol = (uint16_t)adc_data[1] * ADC_VREF / 4095U; printf("\r\n ADC1_AIN1: ADC Count: 0x%03x, ADC Input Voltage = %d.%02d V \r\n", (uint16_t)adc_data[1], (int)adc_inp_vol, (int)((adc_inp_vol - (int)adc_inp_vol)*100.0)); } if (adc_ch2_done == true) { adc_ch2_done = false; adc_inp_vol = (uint16_t)adc_data[2] * ADC_VREF / 4095U; printf("\r\n ADC1_AIN2: ADC Count: 0x%03x, ADC Input Voltage = %d.%02d V \r\n", (uint16_t)adc_data[2], (int)adc_inp_vol, (int)((adc_inp_vol - (int)adc_inp_vol)*100.0)); } } /* Execution should not come here during normal operation */ return ( EXIT_FAILURE ); }
Polling mode:
#include <stddef.h> // Defines NULL #include <stdbool.h> // Defines true #include <stdlib.h> // Defines EXIT_FAILURE #include "definitions.h" // SYS function prototypes #define ADC_VREF (3.3f) // ***************************************************************************** // ***************************************************************************** // Section: Main Entry Point // ***************************************************************************** // ***************************************************************************** uint32_t adc_data; float adc_inp_vol; int main ( void ) { /* Initialize all modules */ SYS_Initialize ( NULL ); while ( true ) { ADC_GlobalEdgeConversionStart(); while (ADC_ChannelResultIsReady(ADC_CORE_NUM1, ADC_CH0) == false); adc_data = ADC_ResultGet(ADC_CORE_NUM1, ADC_CH0); adc_inp_vol = (uint16_t)adc_data * ADC_VREF / 4095U; printf("ADC1_AIN0: ADC Count: 0x%03x, ADC Input Voltage = %d.%02d V\r", (uint16_t)adc_data, (int)adc_inp_vol, (int)((adc_inp_vol - (int)adc_inp_vol)*100.0)); } /* Execution should not come here during normal operation */ return ( EXIT_FAILURE ); }
Library Interface
ADC Controller peripheral library provides the following interfaces:
Functions
| Name | Description |
|---|---|
| ADCx_Initialize | Initializes given instance of ADC peripheral |
| ADCx_Enable | Enables the ADC module |
| ADCx_Disable | Disables the ADC module |
| ADC_CompareEnable | Enables digital comparisons for the given channel on the specified ADC core |
| ADC_CompareDisable | Disables digital comparisons for the given channel on the specified ADC core |
| ADC_CompareWinThresholdSet | Configures the low and high threshold values for the comparator on the specified ADC core |
| ADC_CompareWinModeSet | Configures the low and high threshold values for the comparator on the specified ADC core |
| ADC_GlobalInterruptsStatusGet | Returns the global interrupt status |
| ADC_CoreInterruptsEnable | Enables the specified ADC core's interrupt |
| ADC_CoreInterruptsDisable | Disable the specified ADC core's interrupts |
| ADC_CoreInterruptsStatusGet | Returns the specified ADC core's interrupt status |
| ADC_CoreInterruptsStatusClear | Clears the specified ADC core's interrupt status |
| ADC_GlobalEdgeConversionStart | Generates global edge trigger and starts conversion on channels configured with Global edge as the trigger source |
| ADC_GlobalLevelConversionStart | Starts global level trigger and starts conversion on channels configured with Global level as the trigger source |
| ADC_GlobalLevelConversionStop | Stops global level trigger and stops conversion on channels configured with Global level as the trigger source |
| ADC_SyncTriggerEnable | Enables sync trigger defined by CTRLC.CNT value |
| ADC_SyncTriggerDisable | Disables sync trigger |
| ADC_SyncTriggerCounterSet | Configures the value of CTRLC.CNT register |
| ADC_SoftwareControlledConversionEnable | Enables software controlled conversion on the specified ADC core's channel |
| ADC_ChannelSamplingStart | Enables the Analog Mux Input and starts sampling on the ADC core and channel that was specified using the ADC_SoftwareControlledConversionEnable() API |
| ADC_ChannelSamplingStop | Stops sampling on the ADC core and channel that was specified using the ADC_SoftwareControlledConversionEnable() API |
| ADC_ChannelConversionStart | Starts conversion on the ADC core and channel that was specified using the ADC_SoftwareControlledConversionEnable() API |
| ADC_ChannelResultIsReady | Indicates whether ADC conversion is complete on the specified ADC core's channel |
| ADC_EOSStatusGet | Indicates whether End of scan interrupt flag is set on the specified ADC core |
| ADC_ResultGet | Returns the ADC conversion value for the specified ADC core channel |
| ADC_FIFORead | Returns a single ADC conversion value from the ADC FIFO |
| ADC_FIFOBufferRead | Returns multiple ADC conversion values from the ADC FIFO |
| ADC_GlobalCallbackRegister | Registers the global callback function |
| ADC_COREnCallbackRegister | Registers the ADC core specific callback function |
Data types and constants
| Name | Type | Description |
|---|---|---|
| ADC_CORE_INT_CMPHIT | Macro | Identifies ADC core interrupt status |
| ADC_FIFO_CORID_GET | Macro | Returns the ADC core id in the ADC FIFO data |
| ADC_FIFO_DATA_GET | Macro | Returns the ADC conversion resunt from the ADC FIFO data |
| ADC_FIFO_CHNID_GET | Macro | Returns the ADC channel id in the ADC FIFO data |
| ADC_FIFO_CNT_GET | Macro | Returns the current number of entries present in the ADC FIFO |
| ADC_GLOBAL_INT_CRRDY1 | Macro | Identifies ADC global interrupt status |
| ADC_CHANNEL_NUM | Enum | Identifies ADC channel number |
| ADC_CORE_NUM | Enum | Identifies ADC core |
| ADC_CORE_CALLBACK | Typedef | Defines the function pointer data type and function signature for the adc peripheral core callback function |
| ADC_GLOBAL_CALLBACK | Typedef | Defines the function pointer data type and function signature for the adc peripheral global callback function |
| ADC_CORE_CALLBACK_OBJECT | Struct | ADC Core events Callback structure |
| ADC_GLOBAL_CALLBACK_OBJECT | Struct | ADC Global Callback structure |