2.3.44 ADC_FIFORead Function
C
uint32_t ADC_FIFORead(void)
Summary
Returns a single ADC conversion value from the ADC FIFO
Description
Returns a single ADC conversion value from the ADC FIFO
Precondition
ADCx_Initialize() function must have been called first for the associated instance.
Parameters
None
Returns
uint32_t - ADC result value
Example
uint32_t adc_result;
if (ADC_EOSStatusGet(ADC_CORE_NUM1))
{
// ADC conversion is complete. Read the conversion result.
adc_result = ADC_FIFORead();
}
Remarks
None