2.3.47 ADC_GlobalInterruptsStatusGet Function
C
ADC_GLOBAL_INT ADC_GlobalInterruptsStatusGet(void)
Summary
Returns the global interrupt status
Description
This function returns the global interrupt status
Precondition
ADCx_Initialize() function must have been called first for the associated instance.
Parameters
None
Returns
ADC_GLOBAL_INT - bitwise OR of the following macros indicating global interrupt event status: ADC_GLOBAL_INT_PFFHFUL ADC_GLOBAL_INT_PFFRDY ADC_GLOBAL_INT_PFFOVF ADC_GLOBAL_INT_PFFUNF ADC_GLOBAL_INT_VREFRDY ADC_GLOBAL_INT_VREFUPD ADC_GLOBAL_INT_CRRDY1
Example
ADC_GLOBAL_INT adcGlobalIntStatus; adcGlobalIntStatus = ADC_GlobalInterruptsStatusGet();
Remarks
None