14.4.6.3 Data Interpretation
The BATMON_OK bit in the BATMON register (BATMON.BATMON_OK) monitors the current value of the battery voltage:
- If BATMON_OK = 0, the battery voltage is lower than the threshold voltage
- If BATMON_OK = 1, the battery voltage is higher than the threshold voltage
After setting a new threshold, the value BATMON_OK should be read out to verify the current supply voltage value.
Note: The battery monitor is inactive during P_ON, and SLEEP states, see the TRX_STATUS bits
in the TRX_STATUS register (TRX_STATUS.TRX_STATUS).