4.4.2.3 Create Example Project
Select File>New Project or the New Project icon
to
open the Project wizard. Follow the steps below to create your project. Click
Next to move to the next step.
- Choose Project: Click on the “Microchip Embedded” category and then the “Standalone Project” project.
- Select Device (and Tool): Enter the device “AVR128DA48.” Then enter the tool “AVR128DA48 Curiosity Nano-SN: MCHPL#” where the tool serial number (SN) contains the prefix “MCHP” followed by a multi-digit number.
- Select Compiler: Under Compiler Toolchains>XC8, select the version used in this example or the most-current version.
- Select Project Name and Folder: Name your project. For example, “Hello World Debug GPIO.” For Windows OS, the default project folder is C:\Users\<UserName>\MPLABXProjects.
After clicking Finish, the project tree should appear in the Projects window.