4.8.2.2.5 Radio Group

The Radio Group widget is a group of radio buttons where only one option can be selected at any time. Initially the first option is selected.

To make changes to the list, use the editor under Values.

You can also display the options horizontally.

Data Fields

The Radio Group widget has a source data field. Each time the state of the widget is changed a value is sent.

Configuration

Hover over parameters in visualizer for more information.

Table 4-37. Radio Group
ParameterTypeUsage
ValuesEditorEdit a list of options to name, add, delete or rearrange options.
HorizontalCheck boxCheck to display options horizontally.
Table 4-38. Font Group
Parameter Type Usage
Font Size Numeric Enter font size
Font Weight Dropdown box Select the font weight (such as bold)
Font Style Dropdown box Select the font style (such as italics)
Font Family Dropdown box Select the font family (such as segment)