4.8.2.2.2 Button

The Button widget will send a value each time it is pressed. The button can either be configured as a normal push button or as a toggle button. The button can have a static text to indicate its functionality.

When it is configured as a toggle button the text will be replaced by ON or OFF depending on the state of the button. To replace the ON/OFF text by something else the Text parameter must be given as '/' delimited text with the first part of the text being the ON state text and the second part the OFF state text. For example, "CLICKED/UNCLICKED."

Data Fields

The Button widget has a source data field. Each time the button is pressed a packet is sent. The value of the packet will always be:
  • 0 for a normal push button
  • Either 0 for a toggle button in its OFF state or 1 for a toggle button in its ON state. So if a button in the OFF state is pressed, the value will change to the ON state and vice versa.

Configuration

Hover over parameters in visualizer for more information.

Table 4-29. Button Group
ParameterTypeUsage
LabelTextEnter label text.
ModeDropdown boxSelect Fixed or Toggle.
ValueNumericIf Mode is Fixed, Enter the value sent when button pressed.
Table 4-30. Colors Group
Parameter Type Usage
Foreground Color selection dialog Color of widget foreground.
Background Color selection dialog Color of widget background.
Table 4-31. Font Group
Parameter Type Usage
Font Size Numeric Enter font size
Font Weight Dropdown box Select the font weight (such as bold)
Font Style Dropdown box Select the font style (such as italics)
Font Family Dropdown box Select the font family (such as segment)
Table 4-32. Alignment Group
Parameter Type Usage
Horizontal Dropdown box Select the horizontal alignment of content
Vertical Dropdown box Select the vertical alignment of content
Line Wrap Dropdown box Select conditions to wrap line of content