Escape Mode
Escape mode uses the data lanes to communicate asynchronously using the low-power states at low speed. The D-PHY supports this mode in both directions. A data lane enters Escape mode through an Escape mode entry procedure (LP-11, LP-10, LP-00, LP-01, LP-00), if an LP-11 is detected before reaching LP-00 state, the entry is aborted and the receiver returns to the Stop state. Once the sequence is correctly completed, the transmitter sends an 8-bit command to indicate a requested action.
If the entry command is not valid, it is ignored, the error flag ERRESC goes high (DSI_INT_ST0.DPHY_ERRORS_0), and the receiver waits until the transmitter returns to the Stop state.
The D-PHY applies Spaced-One-Hot encoding (a Mark state is interleaved with a Space state) on commands and data. Each symbol consists of the following two parts:
- One-Hot phase
- Space state
To transmit one bit, a Mark-1 should be sent followed by the Space state. In the case of a zero bit, a Mark-0 should be sent followed by the Space state.
| Escape Mode Action | Entry Command Pattern (First Bit to Last Bit to be Transmitted) | Command Type |
|---|---|---|
| Low-Power Data Transmission | 11100001 | Mode |
| Ultra-Low-Power State | 00011110 | Mode |
| Reset Trigger | 01100010 | Trigger |
| Unknown - 3 | 01011101 | Trigger |
| Unknown - 4 | 00100001 | Trigger |
| Unknown - 5 | 10100000 | Trigger |
The Escape mode transition sequencing from state to state is presented in Figure 7-4.
- Low-Power Data Transmission (LPDT)
In LPDT mode, the data can be transmitted by the protocol at low speed in Low-Power mode. High-speed drivers or receivers are off and low-power drivers or receivers are on. During LPDT, the protocol can pause by maintaining a Space state on the lines.
- Remote Trigger
Remote Trigger mode allows the protocol to send a flag to the receiving side, at the request of the transmitting side.
- Ultra-Low-Power State (ULPS)
Ultra-Low-Power State (ULPS) mode has the lowest power consumption, excluding Shutdown mode.
For data lanes, this mode is entered by sending an Ultra-Low-Power state entry command after the Escape mode entry command. During this mode, the lines are in the Space state (LP-00). Although the clock lane does not support regular Escape mode, the clock lane supports ULPS. If all lanes are set to ULPS, the PLL is turned off.
- Turnaround
The D-PHY allows the transmission direction of the data lanes to be swapped by means of a turnaround request. The sequence of a turnaround operation is described below:
- Transmitter side
- Starts when the DSI host initiates a turnaround request, assuming the D-PHY is in Stop state
- The transmitter sends specific low-power sequence—LP-11, LP-10, LP-00, L-10, L-00 The turnaround operation can be disabled while in power down mode.
- Receiver side
- After receiving a complete low-power sequence, the receiver enables the low-power driver.
- Transmits LP-00, indicating change.
- Overlapping LP-00 transmitted by the initial transmitter.
- Initial receiver side transmits LP-10, followed by LP-11, returning to Control mode.