1.5 Instantiating MiV ESS Core
(Ask a Question)To instantiate the MiV ESS core, perform the following steps:
- From the Catalog, drag the MiV ESS IP core to SmartDesign.
- In the Create Component dialog box, enter MIV_ESS_C0 as the component name, and click OK.
- In the MiV ESS Configurator screen, perform the following configurations:
- Navigate to General tab, and make sure that the configurations are same as shown in the following figure.
- Deselect Bootstrap
- Select the following peripherals: GPIO and UART and deselect all others.
Figure 1-12. General Configurator - Navigate to APB tab, and make sure that the configurations are same as shown in the following figure.
- Select APB Mirrored I/F
- External APB Target: Slot 3 and Slot 4
Figure 1-13. APB Configurator - Navigate to GPIO tab, and make sure that the configurations are same as shown in the following figure.
Figure 1-14. GPIO Configurator - Navigate to UART tab, and make sure that the configurations are same as shown in the following figure.
Figure 1-15. UART Configurator
- Navigate to General tab, and make sure that the configurations are same as shown in the following figure.
- To generate the component, click OK.