37.2.4.2 I3C Address Header
The I3C Address Header follows either a Start or a Restart condition and follows the same format as an I2C Address Header – 7 Address bits, one R/W bit, and one ACK/NACK bit.
The Address Header following a Start Condition (but not a Restart condition) is subject to arbitration. This means that multiple devices may be attempting to drive an address on the bus using the SDA lines and is, therefore, transmitted in Open-Drain mode. Refer to I3C Address Arbitration for more information.
The Address Header following a Restart condition is not subject to any arbitration, meaning only the Controller drives an address on the bus and is, therefore, always transmitted in Push-Pull mode with the exception of ACK/NACK bit. Figure 37-10 shows a non-arbitrable Address Header in Push-Pull mode.
0) to represent Write mode (the Controller writing to the Target).
The device transmits a high signal on SDA line (R/W bit =
1) to represent Read mode (the Controller reading from the Target).
The R/W bit follows the same signaling (Open-Drain or
Push-Pull) as that of the 7 Address bits preceding it. In a Private I3C/I2C
Transaction, the status of the R/W bit is captured in the RNW bits.Once the device transmits the first eight bits of the address header on the bus, it waits
for the other device (the Controller waits for the Target, the Target waits for the
Controller) to acknowledge (or not acknowledge) the request. This is done through the
ninth ACK/NACK bit in the address header. The
ACK/NACK bit is always transmitted in Open-Drain regardless
of the signaling used to transmit the first eight bits. The responding device pulls the
SDA line low (ACK/NACK bit = 0) to respond
with an acknowledge (ACK), whereas the responding device
releases the SDA line high (ACK/NACK bit = 1)
to respond with a non-acknowledge (NACK). Table 37-6 shows the different conditions when this Target module ACKs and
NACKs an address on the bus.
| Transaction | ACK Condition | NACK Condition |
|---|---|---|
| Broadcast Address | Always | Never |
| Private/I2C Read Transaction(1) |
Or, once when ACKP =
1 and ACKPOS = 1 in addition to data being
ready to be transmitted from the TX FIFO (TXFNE =
1) |
Always when TX FIFO is empty (TXFNE = Or, always when ACKP = |
| Private/I2C Write Transaction(1,2) |
Always when ACKP = Or, once when ACKP = |
Always when ACKP = |
| ENTDAA Dynamic Address Assignment |
Always when HJCAP =
0 and Target does not have a
Dynamic Address assignedOr, only after Hot-Join has been requested when HJCAP =
|
Before Hot-Join has been requested when HJCAP =
Or, any time the Target already has an assigned Dynamic Address |
|
Note:
|
||
The following address types can be transmitted on the I3C bus:
- I2C Static Address
- I3C Dynamic Address
- I3C Broadcast Address
- I3C Hot-Join Address