5.3.5.8 Unbond Device or Unbond

Table 5-56. Format
Firmware Version 1.0Firmware Version 1.2 and Later
U,<1-8,Z>

UB,<1-8,Z>

Note: All firmware version 1.0 syntax remains valid in version 1.2 and later.

Command U or UB removes existing bonding. This command works in both central or peripheral GAP roles.

Command U or UB expects one input parameter. The parameter indicates the index of the bonding that needs to be removed. Use command LB to determine the index of the bonding. If the input parameter is the letter Z, then all bonding information is cleared. If an empty index is available, the new pairing and bonding information is added at the first available empty index.

ItemFirmware Version 1.0 and LaterDescription
Example:U,1Remove the bond with index 1
Response:AOKSuccess
ErrSyntax error or invalid parameter
ItemFirmware Version 1.2 and LaterDescription
Example:UB,1Remove the bond with index 1
Response:AOKSuccess
ErrSyntax error or invalid parameter