5.3.5.5 Add Bonded List Into Accept List or Accepted List by Bonded Device

Table 5-53. Format
Firmware Version 1.0Firmware Version 1.2 and Later
JB

ALB

Note: All firmware version 1.0 syntax remains valid in version 1.2 and later.

Use command JB or ALB to add all currently bonded devices to the accept list. Command JB or ALB does not expect any parameter.

The random address in the accept list can be resolved with command JB or ALB for connection purpose. If the peer device changes its resolvable random address, the RNBD350 module is still able to detect that the different random addresses are from the same physical device and, therefore, allows a connection from such a peer device. This feature is particularly useful if the peer device is an iOS or Android device that uses a resolvable random address.

ItemFirmware Version 1.0 and LaterDescription
Default:None
Example:JBAdd all bonded devices to accept list
Response:AOKSuccess
ItemFirmware Version 1.2 and LaterDescription
Default:None
Example:ALBAdd all bonded devices to accept list
Response:AOKSuccess