2.2 Creating a New SmartDesign Component
(Ask a Question)To create a new SmartDesign component:
- In Libero, select .
- In the Create New SmartDesign dialog box, enter
top as the name of the new SmartDesign project, as shown in
the following figure.
Figure 2-3. Create New SmartDesign
- Click OK.
The top SmartDesign component is created.