To generate the SmartDesign component, perform the following steps:
In Design Hierarchy, right-click top, and select Set
As Root.
Save the project.
Click the Generate
Component icon (shown in the following figure) on the SmartDesign
toolbar.Figure 2-24. Generate Component IconWhen the Mi-V component is generated, the Message window
displays the message, “The top was generated successfully.”
Important: In case any error is observed related to address space access issue,
ensure to perform the following step: Navigate to Project > Project Settings > SmartDesign, and then Enable "Downgrade memory map generation DRC errors to
warnings" as shown in the following figure.Figure 2-25. Project Settings
Select the Build Hierarchy option and save the project.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.